This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C5545: C5545 BoosterPack Software document

Part Number: TMS320C5545


Tool/software: Code Composer Studio

I want to know in the C5545 BoosterPack Software document 3.3.3.2-step2 and 3. Which path are they refer to? Are they are in the pictures I show in the below?

The file names are a little different. I am not sure. 

  • Hi Yutong,

    It is possible to have some mismatch in C5545 BoosterPack Software User's Guide (sprui92.pdf) because it is since 2016 but the describe folders at points 2 and 3 seems refer to CSL Out of Box Demo as it is described in the section 1.2 of the same guide.
    c55xCSL can be downloaded at:
    http://www.ti.com/tool/sprc133
    The right path to described folders:
    c5545BoostEqualizer
    c5545BoostEqualizerProfile
    is
    ..ti/c55_lp/c55_csl_3.08/demos/out_of_box/c5545/c5545bp_software_01.01.00.00/source_code/c5545bp_ble_firmware/

    Regards,
    Tsvetolin Shulev