Part Number: DRV8312-69M-KIT
Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE
Tool/software: Code Composer Studio
Dear Sir/Madam
I had DRV8312-69M kit with BLDC motor, I installed CCSv8 and also latest versions of controlsuit and motorware. I took project from controlsuit C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\BLDC_Sensored make changes in configuration and build it successfully and I run C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\~GUI, In this GUI target is detected but DC bus voltage is not getting detected(shows yellow light) so im not able to enable the motor. I made all hardware setting as per mentioned in the document.
Is this is correct way to run DRV8312-69M kit GUI???
Please suggest if anything wrong in the procedure or if something else has to be done.