This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP-EXP432P401R: cannot find .obj .hex .d file on compiling

Part Number: MSP-EXP432P401R


Tool/software: Code Composer Studio

Hi, I want to test out empty_MSP_EXP432P401R_tirtos_ccs project mentioned in http://dev.ti.com/tirex/#/?link=Software%2FSimpleLink%20MSP432P4%20SDK%2FSimpleLink%20Academy%2FTI%20Drivers%2FConfiguring%20TI%20Drivers with newly installed CCS 8.3 version. But after the hammer button was clicked just after the project was imported, the console will output:

Buildfile generation error occurred..
Cannot build project. Referenced RTSC Configuration project 'tirtos_builds_MSP_EXP432P401R_release_ccs' contains build-errors.
Build stopped..

And when I do this at second and third time, there will be more output.

**** Clean-only build of configuration Debug for project empty_MSP_EXP432P401R_tirtos_ccs ****

"D:\\Program Files\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 clean -O 
 
DEL /F  "empty_MSP_EXP432P401R_tirtos_ccs.hex"  "empty_MSP_EXP432P401R_tirtos_ccs.out" 
DEL /F "MSP_EXP432P401R.obj" "empty.obj" "main_tirtos.obj" 
DEL /F "MSP_EXP432P401R.d" "empty.d" "main_tirtos.d" 
Cannot find D:\test\empty_MSP_EXP432P401R_tirtos_ccs\Debug\empty_MSP_EXP432P401R_tirtos_ccs.hex
Cannot find D:\test\empty_MSP_EXP432P401R_tirtos_ccs\Debug\MSP_EXP432P401R.obj
Cannot find D:\test\empty_MSP_EXP432P401R_tirtos_ccs\Debug\MSP_EXP432P401R.d
Finished clean
 

**** Build Finished ****
Buildfile generation error occurred..
Cannot build project. Referenced RTSC Configuration project 'tirtos_builds_MSP_EXP432P401R_release_ccs' contains build-errors.
Build stopped..

I have tried this process several times and with different workspaces, but things have never worked. Also I noticed IDE seems call DEL command to remove these later not found files. I failed to find similar issues on the web so I am here to ask for suggestion. Thanks.

  • Hello,
    The dependent TI-RTOS project failed to build. Can you provide all the build messages from the project? It should be in the build console when you select that project in the Project Explorer.

    Thanks
    ki
  • So here is what I get when build the tirtos_builds_MSP_EXP432P401R_release_ccs project:

    **** Build of configuration Debug for project tirtos_builds_MSP_EXP432P401R_release_ccs ****
    
    "D:\\Program Files\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O 
     
    making ../src/sysbios/sysbios.aem4f ...
    gmake[1]: Entering directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    asmem4f D:/PROGRA~1/ti/simplelink_msp432p4_sdk_2_40_00_10/kernel/tirtos/packages/ti/sysbios/family/arm/m3/IntrinsicsSupport_asm.sv7M ...
     
    >> Compilation failure
    makefile:50: recipe for target 'm3_IntrinsicsSupport_asm.obj' failed
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/clock.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/mqueue.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread_barrier.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread_cond.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread_key.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread_mutex.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread_rwlock.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/pthread_util.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/sched.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/semaphore.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/sleep.c', needed by 'BIOS.obj'.
    gmake[1]: *** No rule to make target 'ti/posix/tirtos/timer.c', needed by 'BIOS.obj'.
    Fatal error: cannot open source file "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs"
    1 catastrophic error detected in the compilation of "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs".
    Compilation terminated.
    gmake[1]: *** [m3_IntrinsicsSupport_asm.obj] Error 1
    Fatal error: cannot open source file "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs"
    1 catastrophic error detected in the compilation of "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs".
    Compilation terminated.
    gmake[1]: *** [m3_Hwi_asm.obj] Error 1
    gmake[1]: Leaving directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    gmake[1]: Entering directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    asmem4f D:/PROGRA~1/ti/simplelink_msp432p4_sdk_2_40_00_10/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M ...
     
    >> Compilation failure
    makefile:42: recipe for target 'm3_Hwi_asm.obj' failed
    Fatal error: cannot open source file "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs"
    1 catastrophic error detected in the compilation of "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs".
    Compilation terminated.
    gmake[1]: *** [m3_Hwi_asm_switch.obj] Error 1
    Fatal error: cannot open source file "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs"
    1 catastrophic error detected in the compilation of "Files/ti/simplelink_msp432p4_sdk_2_40_00_10/source/ti/posix/ccs".
    Compilation terminated.
    gmake[1]: *** [m3_TaskSupport_asm.obj] Error 1
    gmake[1]: Target 'all' not remade because of errors.
    gmake[1]: Leaving directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    gmake[1]: Entering directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    asmem4f D:/PROGRA~1/ti/simplelink_msp432p4_sdk_2_40_00_10/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm_switch.sv7M ...
     
    >> Compilation failure
    makefile:46: recipe for target 'm3_Hwi_asm_switch.obj' failed
    gmake[1]: Leaving directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    gmake[1]: Entering directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    asmem4f D:/PROGRA~1/ti/simplelink_msp432p4_sdk_2_40_00_10/kernel/tirtos/packages/ti/sysbios/family/arm/m3/TaskSupport_asm.sv7M ...
     
    >> Compilation failure
    makefile:54: recipe for target 'm3_TaskSupport_asm.obj' failed
    gmake: *** [../src/sysbios/sysbios.aem4f] Error 2
    gmake[1]: Leaving directory 'D:/test/tirtos_builds_MSP_EXP432P401R_release_ccs/src/sysbios'
    ../src/makefile.libs:56: recipe for target '../src/sysbios/sysbios.aem4f' failed
    gmake: Target 'all' not remade because of errors.
    
    **** Build Finished ****
    

    Could you please explain what should I do to resolve this?

  • Thanks.

    This is the issue:

    user5964221 said:
    "D:\\Program Files\\ti\\ccsv8\\utils\\bin\\gmake"

    You installed CCS (and other software packages like the SDK) inside a folder with spaces.

    See the below link:

    http://software-dl.ti.com/ccs/esd/documents/sdto_ccs_build-errors.html#general

    Specifically this part: 

    A space/whitespace character, while acceptable in most cases, can cause build issues with SYS/BIOS projects, hence it is recommended to also avoid it.

    Your dependent SYS/BIOS project is failing to build.

    Thanks

    ki