This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCSv8.3, Resource Explorer encountered a problem



Tool/software: Code Composer Studio

Hi,

I have had this issue for some time now, when trying to open Resource Explorer inside CCS. Error message: 

Resource Explorer encountered a problem. Please close and reopen Resource Explorer. 

[] Running with Window 7 64-bit

[] Went through the Troubleshooting for Resource Explorer, made sure proxy is set to native, restarted CCS twice

[] Removed the tirex-localserver-* to force it to recreate

[] Re-installed CCSv8.3

[] Using an open internet connection

[] verified when CCS is closed, that there is no "node" in task manager. When CCS  starts fresh, there is still no "node". When trying to start TIREX, then there are 2x "node.exe" in task manager.

[] tried to make sense of the tirex-xxxx.log

Could you let me know what else to try?

I am attaching the .logs file.

tirex-2019-03-14.txt

Thanks,

--Gunter