This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6655: CCS6.2 (using XDS 200 debugger): Can not set breapoints at a specific code line for debug

Part Number: TMS320C6655

Tool/software: Code Composer Studio

Hi 

I've tried to set breakpoints on CCS debug. But every time I've tried to set a breakpoint at a specific line of code then the debugger jumps to the start a a sub-routine and set the breakpoint there.

I'm using the compile version for C6000, 7.4.12 with no optimization (-O0, --symdebug:dwarf)

CCould it be some compiler option I should use?

Can you please help

BR

Tam Tran

Vestas Wind System