Part Number: TMS320F2808
Tool/software: Code Composer Studio
Hello,
I have picked up an old project that is using the CL2000 compiler version 3.09.
It is also using an old version of CCS, but I have brought the code into the latest CCS, 8.3.0.
With this I am using the latest compiler 18.1.4, but would like to use 3.09, at least for a while.
Is it possible to make CCS discover such an old compiler?
Using Preferences -> Compilers I have discovered others, back to v6.1.0, which (excluding 3.09) is the oldest on my PC (Windows 10, 64-bit).
Perhaps it is just too old?
Regards, Giles