This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi!
When I create a CCS project and deselect "Use default build command" and "Generate Makefiles automatically" I do not seem to be able to acquire the name of the active configuration (such as Debug, Release, or what ever I decide to name it). It is important to get this information since CCS assumes that I put the artifacts into a folder with the same name, so I need to be able to put them there in my custom build script. The intuitive solution would be an exported environment variable, such as ACTIVE_CONFIGURATION=Debug.
I tried to define it automatically with some arbitrary named variable from the view -> Project Properties -> Build -> Variables, but they don't seem to be exported either.... Which seems very counter intuitive in itself.
Is there a work around and will you implement this feature through preferably both functions mentioned above?
BR,
~Johan
Johan Eriksson50 said:When I create a CCS project and deselect "Use default build command" and "Generate Makefiles automatically" I do not seem to be able to acquire the name of the active configuration (such as Debug, Release, or what ever I decide to name it).
When you de-select "Generate Makefiles automatically" the Variables button should become enabled. You should be able to click on it and select a variable. I think config_name might be the one you are looking for.
I found an Eclipse reference on it here: https://help.eclipse.org/kepler/index.jsp?topic=%2Forg.eclipse.cdt.doc.user%2Freference%2Fcdt_u_prop_build.htm
Hope this helps.
Hello AartiG!
Do you mean that I should populate the field "Build command" or the field "Build directory" with this variable?
I tried populating both of these fields, but none of them seem to work. It did not register. Is it maybe the wrong variable?
Johan Eriksson50 said:Do you mean that I should populate the field "Build command" or the field "Build directory" with this variable?
I thought you were looking to populate the "Build directory" with a path that makes use of the variable (that resolves to the name of the build configuration).
Perhaps you could try the ConfigName variable.
Personally I haven't tried such a scenario myself as I work more with the managed make environment that uses the auto-generated makefiles.
Also, for general Eclipse questions like this you might even find some good tips on the internet from other users who may have tried something similar.