Other Parts Discussed in Thread: MSP430FR5994
Tool/software: Code Composer Studio
I noticed a behavor of fprintf under the TI compiler v18.12.1.LTS on an MSP430fr5994.
Normal including stdio.h and stdlib.h the fprintf(stdout,char *); does not product an output on the console. However after reading the tips for using printf, http://software-dl.ti.com/ccs/esd/documents/sdto_cgt_tips_for_using_printf.html, I tried the unbuffered setting;
setvbuf(stdout, NULL, _IONBF, 0); // turn off buffering for stdout
Now, it works.
I don't need this statement with GNU compiler v7.3.2.154. using exactly the same code.
stderr does not seem to be affected, probably because it is unbuffered.
test code follows:
#include <msp430.h>
#include "msp430fr5994.h"
#include <stdlib.h>
#include <stdio.h>
#include "print.h"
/**
* main.c
*/
int main(void)
{
int i= 0;
char test[]="standard test\n";
char errtest[]="error test\n";
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
setvbuf(stdout, NULL, _IONBF, 0); // turn off buffering for stdout
fprintf(stdout,test);
fprintf(stderr,errtest);
return 0;
}