This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320DM8127: fail to connec to target because of FTDI driver ?

Part Number: TMS320DM8127

Tool/software: Code Composer Studio

Hi Experts,

I"m trying to connect to board DM8127 (Camera Starter Kit). but when I test connection on CCS v8, this message appeared:

I tried to follow some instructions about FTDI driver ,but seem it doesn't work. This is what  was shown when I run FT - PROG : 

i have tried to apply a new template to this device  (namely FT222H). Could this be the reason for all of my trouble ?

Can someone help me with this ? Thanks so much

  • Hi,

    >>i have tried to apply a new template to this device  (namely FT222H). Could this be the reason for all of my trouble ?

    Without much further details, I would guess this is the source of the issue.

    Your FTProg screenshot indicates the device is BLANK, thus not being correctly instantiated for operation as a XDS100v2 Debug Probe.

    That said, the attached template was created from my TMDSCSK8127 board (almost identical to a regular XDS100v2). Please feel free to use it to re-program your FTDI device.

    Hope this helps,

    Rafael

    <?xml version="1.0" encoding="utf-16"?>
    <FT_EEPROM>
      <Chip_Details>
        <Type>FT2232H</Type>
      </Chip_Details>
      <USB_Device_Descriptor>
        <VID_PID>1</VID_PID>
        <idVendor>0403</idVendor>
        <idProduct>A6D0</idProduct>
        <bcdUSB>USB 2.0</bcdUSB>
      </USB_Device_Descriptor>
      <USB_Config_Descriptor>
        <bmAttributes>
          <RemoteWakeupEnabled>false</RemoteWakeupEnabled>
          <SelfPowered>false</SelfPowered>
          <BusPowered>true</BusPowered>
        </bmAttributes>
        <IOpullDown>true</IOpullDown>
        <MaxPower>400</MaxPower>
      </USB_Config_Descriptor>
      <USB_String_Descriptors>
        <Manufacturer>MS</Manufacturer>
        <Product_Description>Texas Instruments Inc.XDS100 Ver 2.0</Product_Description>
        <SerialNumber_Enabled>true</SerialNumber_Enabled>
        <SerialNumber />
        <SerialNumberPrefix>MS</SerialNumberPrefix>
        <SerialNumber_AutoGenerate>true</SerialNumber_AutoGenerate>
      </USB_String_Descriptors>
      <Hardware_Specific>
        <Suspend_DBUS7>true</Suspend_DBUS7>
        <TPRDRV>0</TPRDRV>
        <Port_A>
          <Hardware>
            <UART>true</UART>
            <_245FIFO>false</_245FIFO>
            <CPUFIFO>false</CPUFIFO>
            <OPTO>false</OPTO>
          </Hardware>
          <Driver>
            <VCP>false</VCP>
            <D2XX>true</D2XX>
          </Driver>
        </Port_A>
        <Port_B>
          <Hardware>
            <UART>true</UART>
            <_245FIFO>false</_245FIFO>
            <CPUFIFO>false</CPUFIFO>
            <OPTO>false</OPTO>
          </Hardware>
          <Driver>
            <VCP>true</VCP>
            <D2XX>false</D2XX>
          </Driver>
        </Port_B>
        <IO_Pins>
          <Group_AL>
            <SlowSlew>true</SlowSlew>
            <Schmitt>true</Schmitt>
            <Drive>4mA</Drive>
          </Group_AL>
          <Group_AH>
            <SlowSlew>true</SlowSlew>
            <Schmitt>true</Schmitt>
            <Drive>4mA</Drive>
          </Group_AH>
          <Group_BL>
            <SlowSlew>true</SlowSlew>
            <Schmitt>true</Schmitt>
            <Drive>4mA</Drive>
          </Group_BL>
          <Group_BH>
            <SlowSlew>false</SlowSlew>
            <Schmitt>false</Schmitt>
            <Drive>4mA</Drive>
          </Group_BH>
        </IO_Pins>
      </Hardware_Specific>
    </FT_EEPROM>

  • Thank Rafael, I really appreciate that !