This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F2808: choosing between targets

Part Number: TMS320F2808

Tool/software: Code Composer Studio

Hello

I have 2 TMS320F2808 Explorer Kits (or sometimes one F2808 kit and one F28335 kit) connected to a Windows 10 PC via USB - using the XDS100v2 debug connection.  CCS 8.3.0.

I am programming them with different projects, via one CCS session.

Is there a way to associate a specific project with a specific target?

Currently, when I need to program one, I turn the other off. With both turned on it seems to be just chance which get programmed.  Possibly the first one turned on?

This is true even with different target processors.  When I launch a F28335 debug session, sometimes it will successfully connect to and load the F28335, but sometimes it will try to connect to the F2808, and so fail.

Thanks