Part Number: TMS570LS0714
Tool/software: Code Composer Studio
Hi,
I tried to program custom board tms570ls0714 using xds110 debugger. For the first time, the test connection between XDS110 and Micro controller was successful. and i was able to flash code. However immediately after pressing debug button, Controller went to continuous reset mode (Play button was disabled.) Now, when I try to debug, i get the following errors:
IcePick: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
CortexR4: Failed System Reset: (Error -6306) Failed to connect to PRSC module. (Emulation package 7.0.100.0)
Dap: Error connecting to the target: (Error -241 @ 0x0) A router subpath could not be accessed. A security error has probably occurred. Make sure your device is unlocked. (Emulation package 7.0.100.0)
Dap: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
Kindly Help us resolving this issue.
Thanks and Regards,
Krunal Desai