This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049C: XDS110 debugger session cannot be cancelled when target is not powered

Part Number: TMS320F280049C
Other Parts Discussed in Thread: CODECOMPOSER

Tool/software: Code Composer Studio

Hi all

I experience a problem with CodeComposerStudio 8.3.0.00009 in combination with XDS110 debugger and witih TMS320F280049C 

When I start a debug session everything is fine. When power down the target while the debug session is still running the message appears: 

Trouble Halting Target CPU:
(Error -1156 @ 0x0)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
(Emulation package 8.0.903.2)

This is understandable, because the target has no power. The dialog offers for retry Yes / No / Cancel. Yes and No will retry with different options. What does Cancel do? I would guess, it will cancel the debug session. But it doesn't. The window keeps re-appearing. CodeComposer Studio is blocked unless I re-power the target. 

When I click cancel, for a very brief time the dialog disappears before it re-appears. This gives me enough time to try to click on "terminate" or Ctrl-F2. When I manage to do that before the dialog re-appears. The CCS crashes. ...

Is there a fix for that?

thank you 

Johannes