This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Crash on building project for a CC2640R2F on Debian Testing

Part Number: CC2640R2F

Tool/software: Code Composer Studio

Hi,

when building my project for the CC2640R2F Code Composer Studio freezes sometimes at some point while building/compiling. It seems lik CCS is fully frozen and does not respond on any user inputs. As far as i could check it seems to be something with updating the GUI or similar. When building from command line everything works fine. Even when i open the terminal/console inside CCS in a seperate window it seems to be better (so far). If the console is inside a tabbed panel in the main-window of CCS it seems like breaking much more often.

I've run CCS from command line and couldn't see any messages or error logs. I've noticed that when i kill CCS the workspace is blocked. I can't restart CCS immediately but after a few tries.

Any ideas about the causes? Thanks in advance.

Best regards,
Jan