This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28027: How can I change my default linker command file?

Part Number: TMS320F28027

Tool/software: Code Composer Studio

Hi  Dear, 

I am using CC STUDIO to program C2000 launch pad(LAUNCHXL-F28027). I am using simple example programs from C2000 ware form Resource Explorer. when I get imported from C2000 ware it automatically comes with default linker command file for debugging, which I don't want to. 

I need linker command file flash programming so that I get my piece of code into ROM area instead of any other location.

If my approach is correct to get my code into BOOT ROM, kindly suggest a way to change the default linker command file.

Thanks & Regards 

Himavanth