This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352R: SPI Flash CS pin change

Part Number: CC1352R

Tool/software: Code Composer Studio

Hi Team,

i am working CC1352R1 launchpad SPI Protocal for Flash application. it has on board external Flash with "CC1352R1_LAUNCHXL_SPI_FLASH_CS as IOID_20". i am using other external Fash Memory for more data storage. can i use any GPIO pin as CS like IOID_11. if i can change GPIO what are changes need to do in code driver.