Part Number: AWR1642
Tool/software: Code Composer Studio
The AWR1642 has the maximal 4 profile configures. at first ,I use 3 profiles and the program runs normally, than I add the profiles to 4, the run result is
[C674X_0] {module#39}: line 221: error {id:0x190000, args:[0x81ab30, 0x20]}
xdc.runtime.Error.raise: terminating execution
I get the line 221,it is the HeapMem_alloc() in HeapMem.c
and I also find that the DSS does not go into the MmwDemo_dssMmwaveConfigCallbackFxn , but in the MSS, the return value of MMwave_config() is 0, it is a correct value.
I can't solve the question,who can help me , thank you !