Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hi,
I'm trying to use the CC1310 LaunchPad's external debugger header to program a CC1310 on another board but can't seem to manage a connection.
I've removed all the jumpers from the P4 header and set the VSENSE header to XDS110 Power. When trying to debug the module from ccs, I get the following error message:
Error connecting to the target:
(Error -242 @ 0x0)
A router subpath could not be accessed.
The board configuration file is probably incorrect.
(Emulation package 8.1.0.00007)
Should I change some setting in the Target Configuration file? Note that using the same Target Config settings I'm successfully programming the CC1310 on-board the LaunchPad itself.