Part Number: EVMK2GX
Other Parts Discussed in Thread: 66AK2G12, SYSBIOS
Tool/software: Code Composer Studio
Using the latest everything: CCS (9.0.1), RTOS, ... on Windows 10 machine, Offline Mode.
Just trying to get the ARM (Cortex-A15) RTOS code example running.
When setting up a new CCS Project,
The Target choices are:
"66AK2G12" or "K2GEVM" (K2GEVM seems to work best)
Compiler choice: GNU v7.2.1 (Linaro)
Project Template: SYS/BIOS/GNU Target Examples/Minimal
Protocols and Repositories: Framework Components, k2g PDK, SYS/BIOS, XDAIS
Target: gnu.targets.arm.A15F (preselected)
Platform: the only selectable choice that seems close is "ti.platform.evmTCI66AK2G02"
Build-Profile: "release" is the only option available and is preselected
The Target Configuration File (.ccxml): Basic = "K2GEVM", Advanced (CortexA15) = "evmk2g_arm.gel"
With these selections, the code consists of a main() and "Void taskFxn(UArg a0, UArg a1)"
Build ("Debug") completes without Errors or Warnings and the gel file outputs in Console Window look correct. I can Step and Breakpoint. There is a System_printf statement in main():
System_printf("enter main()\n");
This statement seems to execute; I can step it and all looks good, but there is no output in the Console Window. CIO is "Enabled."
Build Output in Console Window:
**** Build of configuration Debug for project RTOS3 ****
"C:\\TI\\ccs901\\ccs\\utils\\bin\\gmake" -k -j 4 all -O
making ../src/sysbios/sysbios.aa15fg ...
gmake[1]: Nothing to be done for 'all'.
making ../src/sysbios/sysbios.aa15fg ...
gmake[2]: Nothing to be done for 'all'.
**** Build Finished ****
At Debug Start, there is a note for the "... XDS2xx USB Onboard Debug Probe/CortexA15: "0x... (no symbols are defined)"
The gel Console output:
CortexA15: GEL Output: Starting K2G GP EVM Initialization ..
CortexA15: GEL Output: Reading Device Speed from BOOTCFG_EFUSE_BOOTROM
CortexA15: GEL Output: DEVICE SPEED[23:16] ---> 1000 MHz
CortexA15: GEL Output: ARM SPEED[9:0] ---> 1000 MHz
CortexA15: GEL Output: PLL has been configured (24.0 MHz * 250 / 3 / 2 = 1000.0 MHz)
CortexA15: GEL Output: ARM PLL has been configured with ref clock 24MHz, -sysclkp_period 41.6666 (24.0 MHz * 250 / 3 / 2 = 1000.0 MHz)
CortexA15: GEL Output: Power on all PSC modules and DSP domains...
CortexA15: GEL Output: Power on PCIE PSC modules and DSP domains... Done.
CortexA15: GEL Output: UART PLL has been configured (24.0 MHz * 128 / 1 / 8 = 384.0 MHz)
CortexA15: GEL Output: NSS PLL has been configured (24.0 MHz * 250 / 3 / 2 = 1000.0 MHz)
CortexA15: GEL Output: ICSS PLL has been configured (24.0 MHz * 250 / 3 / 10 = 200.0 MHz)
CortexA15: GEL Output: DSS PLL has been configured (24.0 MHz * 198 / 12 / 16 = 24.75 MHz)
CortexA15: GEL Output: XMC setup complete.
CortexA15: GEL Output: DDR3 PLL Setup ...
CortexA15: GEL Output: DDR3 PLL Setup complete, DDR3A clock now running at 533MHz.
CortexA15: GEL Output: DDR3A initialization complete
CortexA15: GEL Output: Entering A15 non secure mode ..
CortexA15: GEL Output: Enabling non-secure access to cp10 and cp11
CortexA15: GEL Output: Enabled non-secure access to cp10 and cp11
CortexA15: GEL Output: Making all GIC interrupts Group1
CortexA15: GEL Output: Changed interrupt group
CortexA15: GEL Output: Set secure mode PMR to non-zero value
CortexA15: GEL Output: Entering NonSecure Mode
CortexA15: GEL Output: Entered NonSecure Mode
CortexA15: GEL Output: A15 non secure mode entered
CortexA15: GEL Output: K2G GP EVM Initialization Complete.
So, now my questions:
1. Why are there no symbols defined?
2. Why is there no print output in the Console Window? (When I did a "bare metal" program, the print out was there. Am I missing a lib? Or, ...
3. Have I made all the correct choices during CCS Project Setup?
thanks,
dave