This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2640R2: How to generate HCI_LE_Connectionless_IQ_Report events for conformance testing

Part Number: LAUNCHXL-CC2640R2

Tool/software: Code Composer Studio

In order to perform the BT5.1 AoA/AoD RF-PHY/RCV/IQC/BV-0X-C phy level tests it is necessary to have an HCI connection to the device under test and the device under test must be able to generate HCI_LE_Connectionless_IQ_Report events. I had hoped to use the example code host_test_app to make an HCI connection to the device and perform these tests. The host_test_app does allow me to make an HCI connection and perform the majority of the phy level tests, however, the device reported features indicate that AoA/AoD is not supported (at least, that's what I think is being returned). Can you confirm that host_test_app does not support AoA/AoD. If so, can you suggest a route which would permit me to perform the AoA/AoD conformance tests? Thank you.