Part Number: CC2640R2F
Other Parts Discussed in Thread: UNIFLASH, , CC2650, LAUNCHXL-CC1352R1
Tool/software: Code Composer Studio
Hi,
I use the SDK "simplelink_cc2640r2_sdk_1_35_00_33" and "simple_peripheral" project under blestack.
I tried to flash both the application and stack binaries using SmartRF Flash Programmer 2 Ver. 1.8.0 and UniFlash (ver. 4.5.0.2056).
Used Debugger - XDS110.
JTAG to the CC2640R2F (Connected JTAG pins TMS, TCK, TDI, TDO and RESET to the BT Chip).
1) In SmartRF Flash Programmer 2,
It detected the target device as CC2640R2F. And connected successfully by right clicking to it (JTAG_Conn_Success_Serial_RF_Flash.jpg).
Then I tried to read the memory from Edit->Address->Read option. And waited some time. Nothing came. It shows the status as "Start reading Flash..." and it went idle. (Mem_Read_Hang_JTAG_Conn_Serial_RF_Flash.jpg)
2) In UniFlash,
Connected device with XDS110 Debug Probe. Tried to read the target device memory from Memory option.
Got error as "(Error -1170 @ 0x0) Unable to access the DAP". (Mem_JTAG_Conn_UniFlash.jpg)
Why it is not reading the memory even the target connected successfully? Is the connection not healthy? If so what could be the reason and how can rectify this?


Thanks and Regards,
Arun