Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138
Tool/software: Code Composer Studio
Te reported error:
Buildfile generation error occurred..
Product 'Inter-processor Communication' v3.47.2.00 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..
In the Project->Properties->General Products Tab, it shows Inter-processor communications 3.47.3.00. And that entry is checked.
The XDC Tools version is 3.51.1.18_core
[com.ti.pdf.omapl138] 1.0.5 shows as "unknown". I will also need the EDMA3 package, but that is a separate issue.
I was able to build the same project with CCS V9, but then found that the emulator I currently have (XDS510), isn't supported in V8. The problems started with V8.
I have completely wiped the installation and re-installed/updated (several times). Tried it in both Linux and Windows, and have similar problems either with this, or the EDMA3 libraries.