Part Number: TMS320F2812
Tool/software: Code Composer Studio
Hi,
I have been using Parallel port for connecting TMS320F2812 target through CC Studio 5.3 (Installed on Win 7 32-Bit OS) and it was working fine.
I was able to Erase, flash, program and debug. But, when I tried the same setup in WIN7 (64-Bit PC), I am not able to even connect the target.
Note : In addition to default CCS 5.3 installation, I have also installed 'setupCCSPlatinum_v30330.exe'
(support.spectrumdigital.com/.../) to enable the connectivity between F2812 target and CCS running in Win 7 (32-Bit PC). Even this driver didnt help for Win-7 64-Bit PC
Please let me know a way forward for this issue.
Or please share us the similar driver that will support Win 7 64-Bit OS.
Thanks and Regards,
R.Balakrishnan