Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Dear all,
I am working with TIVA TM4C1294NCPDT controller in custom made PCB. My project architecture is,
In this project, I need to update the application code (boot loader) of PCB 2 and PCB 3 via PCB 1.
Options available are,
- Through PLC, available in PCB-1
- Through USB stick, available in PCB-1
- Through Ethernet available in PCB-1
Kindly provide your support.
Regards,
Iyyappan.V
iyyappan_krish@yahoo.co.in
+91 8144921242