Part Number: TMDSHVMTRPFCKIT
Tool/software: Code Composer Studio
Ok so we just go the TMDSHVMTRPFCKIT to start testing our HV BLDC motors. the only problem is the card is flashed with the code optimized for running sensorless FOC on ACI and PMSM motors. They have supplied the code for BLDC motors.
The issue I have is that the instructions for reflashing are not very clear but also only correspond to CCS v5 and the current CCS is v9.
I'm assuming I can use the "DC-PwrEntryMacro[M6]" port and power supply included in the box to power just the card and allow reflashing without having to supply mains power to the whole board.
Basically It's just not clear to me how to link CCS v9 to the dev kit and reflash the control card with the BLDC code.