Part Number: AWR1843BOOST
Tool/software: Code Composer Studio
In the project lab0007_medium_range_radar , than I use it to measure the angle ,there are some difference.
I use Rx1 and Rx2 get the angle is -4.9°
the Rx1 and Rx3 get the angle is -4.5°
the Rx1 and Rx4 get the angle is 9.6°
the Rx3 and Rx4 get the angle is -7.4°
the actual angle between radar and object is -5°,
how can I get the correct angle ?