Part Number: CC430F5137
Tool/software: Code Composer Studio
Hi,
So I would like to debug this function and it is called from several places with different buffers.
How do I access the contents of the buffer pointer (& length) from Javascript? Function "transmit" is at 0000ad54 but the parameters (of course) don't show in the map file.
Or do I have to focus on the RF1ADINB register to get data being transmitted?
void transmit(char *buffer, char length)
{
__no_operation();
send_radio_strobe(RF_SCAL); // Calibrate frequency synthesizer and turn it off.
RF1AIES |= BIT9; // High-to-low transition sets interrupt flag
RF1AIFG &= ~BIT9; // Clear pending interrupts
RF1AIE |= BIT9; // Enable TX end-of-packet interrupt
radio_write_multi_bytes_to_register(RF_TXFIFOWR, buffer, length); // Write TX data to radio
__no_operation();
send_radio_strobe(RF_STX); // send_radio_strobe STX
}