This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Scope of access to GPIOs for the two cores in TMS320F28379D

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

Hello,

Please find the below image.There are two different codes in two cores of TMS320F28379D, where InitGpio() function is defined in both the codes. Now when i check, it is given as this function only restricted to one of the core. Does it mean i cannot access GPIOs from both of the cores? Or is it only the InitGpio() function?

Thank you, 

Best Regards,

Sindhu H