Part Number: TMS320F280049
Tool/software: Code Composer Studio
Hello,
can I stamp the linking time like the compile options __time__ and __date__?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
Tool/software: Code Composer Studio
Hello,
can I stamp the linking time like the compile options __time__ and __date__?
Regards, Holger
If you want to somehow use a time stamp while linking, consider using the macro __TIME__. To see the related documentation, please search the C28x assembly tools manual for the sub-chapter titled Linker Command File Preprocessing.
If you want to see when a link was performed, consider using one of these methods. Use the object file display utility ...
% ofd2000 file.out | findstr Time
Time Stamp: Mon Jun 3 10:31:42 2019
The time stamp can also be found in the map file ...
% findstr Linked file.map >> Linked Mon Jun 3 10:31:42 2019
Thanks and regards,
-George
Hello George,
customer is looking for a function which writes the time/date into the file.out code which the application can use.
Regards, Holger
It sound like you want to somehow tell the linker what time stamp to use instead of using the current time. Unfortunately, there is no linker feature which supplies this capability. Further, there is no utility which can change the time stamp in an existing file.out.
Thanks and regards,
-George