Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL, UNIFLASH
Tool/software: Code Composer Studio
I am using TIVA TM4C1294NCPDT controller and TivaWare_C_Series-2.1.4.178. (I am using Launchpad_EK-TM4C1294XL)
Here I can see the flash based boot loader example (UART and demo)
Where can I get the rom based boot loader example?
In flash based boot loader I am having following issue,
1. During app code up gradation, if power fails or any cable disconnection occurs, then we need to download the boot loader via CCS after that only uart boot loader is working via LM flash programming.
If ROM based boot loader is used do I come out of this issue?
Regards,
Iyyappan.V