Tool/software: Code Composer Studio
Hi,
I use the component CC3220MODASF and I have problems reading with I2C the data of 2 sensors: VISHAY VEML6040 and SENSIRION SPS30.
The first problem concern the VISHAY VEML6040, the data has 16 bit registers that need to be addressed without the resending of a stop condition before reading out the sensor. Note below the section I marked with a red arrow , which shows that there should be no stop condition inserted here.
With the SDK I2C API i don't have any input parameter that allows me to control the sending of stop condition within read command, then how can i disable the sending of a stop condition?
The second problem concern the SENSIRION SPS30 that have a 16 bit slave address and the I2C Transfer API allow just 8 bit slave address. how can i communicate with this sensor?
Best regards
Thank you.