This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS ANY VERSION : I CAN'T INSTALL CCS

Tool/software: Code Composer Studio

I'm trying to install Code Composer Studio 9.0.1. but it failed. 

Attach the log file.

Check please..

best regards0361.install_logs.zip

  • Hi,

    A few details that may be affecting yoru ability to install CCS. 

    - Line 3 of the log file <ccs_setup_9.0.1.00004_install.log> shows a "sharp" symbol (#) in the original directory. This symbol is a special character that may be causing the internal installer utilities to fail finding the files. 

    - Line 10 of the same log file above indicates you are installing in a "Program Files" directory - although not in C: but in D:. There is a chance that Windows' User Access Control (UAC) is protecting this directory as well.

    We recommend installing CCS in a directory without spaces and special characters. Also, if you are not doing so, please turn off the Antivirus momentarily during the install procedure. Most Antivirus SW do not cause problems but, since you are experiencing difficulties, it does not hurt trying to disable it. 

    Hope this helps,

    Rafael

  • Thank you! It worked!