Part Number: DRV8301-69M-KIT
Tool/software: Code Composer Studio
Issue with path callout in project source code as per TI kit projects.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8301-69M-KIT
Tool/software: Code Composer Studio
Issue with path callout in project source code as per TI kit projects.
Hi Phillip,
Are you using
1. C2000: the new ROV only supports ELF. Please use the older ROV (called RTOS Object View or ROV Classic depending on your CCS version)
2. Using pre XDCtools 3.50: Again, use the older ROV
If neither of the above apply,
A. does the older ROV work?
B. What versions of CCS, SYS/BIOS, and XDCtools are you using?
C. What compiler and version are you using?
D. How are you loading the image (e.g. CCS).
Todd
Thanks Todd,
1. I did try the ROV Classic.
2. using CCS version 9
3. xdctools_3_55_00_11
4. RTSC error when connecting to target using ROV Classic is that the path is not giving the RTSC configuration package info. What folder and file name.extension to? to point the code composer RTSC configuration tool to?
Any input would be greatly appreciated!
Phil
Phillip,
Can you please right click on the project, select Properties, then click on General. And then click on the “Main” tab, take a snip showing the contents, then click on the “RTSC” tab and take a snip, and then post those to this thread?
Thanks,
Scott