This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Read audio signal form I2S SPH0645LM4H usong CC3220MODASF

Tool/software: Code Composer Studio

Hi,

I am a beginner using I2S protocol and i have some clarification ;

I use an I2S audio Microphone SPH0645LM4H that have 3 pins and i use them to establish connection using I2S with CC3220MODASF:

DOUT connected to   pin64 SD0.

LRLC  connected to   pin63 WS.

BCLK  connected to   pin53 SCK.

I use the default params config of I2S and when i check those param i found that the first one is sampling freq = 1000, what does mean this value? The data Sheet of  SPH0645LM4H indicate that " The Over Sampling Rate is fixed at 64 therefore the WS signal must be BCLK/64 and synchronized to the BCLK. Clock frequencies from 1.024Mhz to 4.096MHz are supported so sampling rates from 16KHz to 64KHz can be had by changing the clock"    how can i translate this to params in the I2S configuration ?

I want to read continuously the audio signal from the SPH0645LM4H Microphone and i don't have an example that help me to extract the signal continuously.

Thanks.

Best regards.