Part Number: TDA2PXEVM
Tool/software: Code Composer Studio
HI,
I want to do cache analysis & profiling of code running on cortex A-15mpu of TDA2PX board. I have already gone through this pdf:- http://www.ti.com/lit/ug/spruhm7b/spruhm7b.pdf which clearly states (1.2 Software and Hardware Requirements) that with XDS560v2 Pro, the Trace Analyzer present can be used for: multicore DSP, AM335x, OMAP3, OMAP4, OMAP5, Cortex-M3, and Cortex-M4 devices. So:
1) is there anything which can be done to do Trace Analyzer for A15 with the same JTAG & CCS.
2) if not then is any other software which can be used to do this analysis on the board during runtime.
Regards
Surbhi