This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO-C2000: What is the scope for setting the pre-defined compilation symbol in CCStudio Version 6.1.3.00034?

Part Number: CCSTUDIO-C2000
Other Parts Discussed in Thread: TMS320F28027

Tool/software: Code Composer Studio

Hi,

We had a problem where the pre-defined symbol on the top level of the project was not picked up within one of the source files at the time of compilation.

After setting one pre-defined symbol at the top of the project, that symbol was not set for one of the files in the project.

Here are two related questions:

1. Is this happening because a possible change of the pre-defined symbols for that file?

2. What is the scope of pre-defined symbols if the procedure below is followed:

- click top of the project

- right click the mouse

- click "Properties" on a pop-up window

- Go to "Build"-"Advanced Options"-"Predefined Symbols"

- click on green icon with "+" and type in the pre-defined symbol

- click OK

- again, right click on the project

- go to top Resources, and click it.

- Click the "Apply" button at the bottom right corner.

Let me know if I am missing something here.

Note that I am using CCS 6.1.3, and that the processor is TMS320F28027, Piccolo.

Regards,

Vlad