Part Number: TMS320C6415
Tool/software: Code Composer Studio
I have 4 TMS320C6415 dsp's connected to the XDS510 PP Plus emulator. I am using Code Composer 3.3. These are all requirements and I cannot change them. In code composer, I use the Parallel Debug Manager. I can connect to all 4 DSPs, open workspaces and load programs to these DSPs. However, when I load our custom .gel file, it tries to write to a specific memory location and cannot. To be clear, I am able to read and write to registers in general despite the gel not loading properly.
The error message is "memory mapping prevented write to target memory 0x........". Another error message I sometimes get is "memory mapping prevented read at target memory 0x..........". Is there a common problem/s that would cause this? How can I write to the memory locations required without this error appearing?