Part Number: MSP430F2274
Tool/software: Code Composer Studio
Hi,
I have a project and I am trying to integrate a boot loader into it.
Currently the boot loader and application are separate files which are then merged manually which is tedious and error prone, it also makes debugging a pain.
I would like to add the boot loader to my normal project but both it and the application are written in C so I would like to be able to duplicate the init code (_c_int00_noargs_noexit).
I see reference online that the source is in the compiler directory, but for me (CCS v9 on OSX) I can't find it - does anyone know where I could obtain a copy?
Thanks.