Part Number: TMS320LF2407A
Tool/software: Code Composer Studio
QUESTION 1: is my device (TMS320LF2407A) supported in CCSv7/8/9. The project was originally built in CCSv3.3
Here is a snippet from the build log that was in the project directory:
QUESTION 2: if this device is still supported, what steps do I need to complete in order to import this project successfully?
When I try to create a new CCSv9 project, I am of course unable to find that device in the list. I get the following error when trying to import the existing project.pjt:
Thank you in advance.