This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Update Code composer Studio v9 from command line



Tool/software: Code Composer Studio

Hello

Is it possible to update the installed features of CCS such as compilers from command line?

We are running CCS v9 on linux docker image and can't use the GUI. The download package contains the version C2000_18.12.1 but we want to use the newest one (C2000_18.12.2).

Many thanks and kind regards,

Tobias