Hi:
I am running into an issue running “any” BIOS program on 6748 EVM, CCS4 with XDS100v1 as well as XDS100v2. It works fine with XDS510USB. Even with XDS100, the code seems to load fine but once loaded, all the menus are disabled in “Target” drop-down. i.e I cannot run, stop etc.. Can I conclude that for running BIOS programs, I will need to use XDS510 ?. I saw a similar discussion here but it was somewhat non conclusive.. http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/54311/192742.aspx#192742
Thanks,
Pradhyum