Part Number: TMS320C6415
Tool/software: Code Composer Studio
Code Composer Studio Parallel Debug Manager seems to have a bug when attempting to run simulations (.out files) on multiple DSPs simultaneously. We are using CCS version 3.3 with the Spectrum digital Emulator, model number XDS510PP Plus. I need to know if there is a workaround for this issue. We need to run simulations on multiple DSPs - The simulation must run simultaneously on each DSP in order for the them to communicate with each other. When clicking the "Run" button in the Parallel Debug Manager the DSPs will run momentarily and then halt. However, when starting each of the DSP's individually, they run continuously but don't stop when they should. Is this a hardware or software issue? If software, what typically causes this?