Tool/software: Code Composer Studio
Hello,
We are using Code Composer Studio 8.3.00009 and load the application .out to AM654x IDK R5F core via the scripting console (we use launch_am65xx.js packaged in Processor SDK 05.02.00.07 release).
We are observing an issue which prevents us from loading the .out continuously (It means that we have to relaunch the target configuration each time).
We suspect the TI Emulator version here. We don't have this problem while using emulator 8.0.903.2 which comes by default with CCS 8.3.00009
Issue started seen with TI emulator version 8.1.0.00012, and can be reproduced with latest 8.2.0.00004 as well
Below is the error description shown in CCS scripting console:
Error loading "....am65xx/05_02_00_10_GA/pdk_am65xx_1_0_3/packages/ti/drv/sciclient/tools/ccsLoadDmsc/am65xx/sciclient_ccs_init_mcu1_0_release.xer5f": Timed out after 20000ms while waiting for target to halt after an auto-run to "main (...\am65xx\loading_.out_file\launch_am65xx_05_02_00_10.js#131)
Could you please check what could be the reason for this issue? Please let us know if you need any additional details regarding our test setup, configuration etc
Regards,
Nijin P