Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
I have DRV8301-HC-EVM Rev D_28069M Kit.
I use the motorware proj_lab12b.
I have a BLDC motor.(20poles = 10 pole pairs)
I have a few questions.
1.
if(EST_getState(obj->estHandle) == EST_State_Rs)
{
ENC_setZeroOffset(encHandle, (uint32_t)(HAL_getQepPosnMaximum(halHandle) - HAL_getQepPosnCounts(halHandle)));
}
Do I not have to use the ENC_setZeroOffset function?
2.
If gMotorVars.Flag_Run_Identify is set to 1, should the electrical angle be 1 to become EST_State_OnLine?
How many electrical angles do you have to be EST_State_OnLine? (0< electrical angles<1)