Tool/software: Code Composer Studio
Hi,
For SDK version: simplelink_cc13x2_26x2_sdk_3_10_01_11, secure commissioning is failing.
- Sensor is successfully associated with coordinator in SM project.
- Association Indication call-back has started secure Commissioning process.
- The two call-backs registered here are smFailCMProcessCb, smSuccessCMProcessCb.
- Always smFailCMProcessCb is being returned during secure commissioning .
- The only changes made are CONFIG_BEACON_ORDER and CONFIG_SUPERFRAME_ORDER to 4 and 4 respectively.
Following log messages are observed on tera term for the SM project
Security module project for collector: collector_sm_CC26X2R1_LAUNCHXL_tirtos_ccs
TI Collector
Restarted
Key Recovery Mode
Channel: 11
PermitJoin-ON
Joined: 0x1
Commissioning Started: 0x1
Sensor 0x1
Commissioning Failed: 0x1
Security module project for sensor: sensor_sm_CC26X2R1_LAUNCHXL_tirtos_ccs
TI Sensor
State Changed: 1
Started: 0x1
Channel: 11
State Changed: 3
Commissioning Started: 0x1
Commissioning Failed: 0x1
State Changed: 5
Anand,
Please forward to the TI support.
Thanks
Sekhar Avutu