This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6657: CCS v9.1 build error.

Expert 2875 points

Part Number: TMS320C6657
Other Parts Discussed in Thread: MATHLIB

Tool/software: Code Composer Studio

Hi,

We are moving to CCS v9.1 from v6.2.

We can success build with CCS v9.1, SYS/BIOS 6.46.06.00 with XDCTools 3.32.01.22.

But when we upgrade SYS/BIOS 6.76.01.12 with XDCTools 3.51.03.28, I got the following errors.

Thanks.

Steve

**** Build of configuration 12AEC for project Project128 ****

 

"C:\\ti\\ccs901\\ccs\\utils\\bin\\gmake" all

Building file: "../app12AEC.cfg"

Invoking: XDCtools

"C:/ti/xdctools_3_51_03_28_core/xs" --xdcpath="C:/ti/dsplib_c66x_3_4_0_0/packages;C:/ti/ipc_3_42_00_02/packages;C:/ti/mathlib_c66x_3_1_1_0/packages;C:/ti/mcsdk_2_01_02_06/demos;C:/ti/pdk_C6657_1_1_2_6/packages;C:/ti/bios_6_76_01_12/packages;C:/P4/dsp/App/60-151x-xx_KomodoDragon_DMP128Plus/Repository;C:/ti/uia_2_00_03_43/packages;C:/ti/xdais_7_24_00_04/packages;C:/ti/xdais_7_24_00_04/examples;C:/ti/edma3_lld_02_11_07_04/packages;C:/ti/ccs901/ccs/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p exC6657 -r release -c "C:/ti/ccs901/ccs/tools/compiler/ti-cgt-c6000_8.3.2" "../app12AEC.cfg"

making package.mak (because of package.bld) ...

generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...

configuring app12AEC.xe66 from package/cfg/app12AEC_pe66.cfg ...

subdir_rules.mk:19: recipe for target 'build-1413783841-inproc' failed

error: xdc.cfg.Program: "C:/ti/xdctools_3_51_03_28_core/packages/xdc/cfg/Program.xs", line 71: xdc.cfg.Program : The package 'ti.sdo.utils' is not compatible with XDCtools used in this build. Please either use XDCtools compatible with that package, or update the product containing that package, or rebuild the package with XDCtools 3.50 or later.

js: "C:/ti/xdctools_3_51_03_28_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!

gmake.exe: *** [package.mak:204: package/cfg/app12AEC_pe66.xdl] Error 1

js: "C:/ti/xdctools_3_51_03_28_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.

gmake[1]: *** [build-1413783841-inproc] Error 1

del Versioninfo.obj