This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/SIMPLELINK-CC3220-SDK: WHAT IS THE PATH FOR 'VALUE' WHILE ADDING VARIABLES IN PREFERENCE

Part Number: SIMPLELINK-CC3220-SDK

Tool/software: Code Composer Studio

hi,

i was going through the previous thread to getting started with CC3220SF.   as demonstrated in documents, to add a variable in the following way,

window -> preference ->  CCS -> Build -> variables -> Add

while adding variable, in 'value'  i could not understand which path i need to add there.

i have tried  this  path .... <SDK> / ... / networktrminal / freertos/ ccs

but still it is throwing the same following error..

**** Build Finished ****
Buildfile generation error occurred..
Cannot build project. Referenced project 'freertos_builds_CC3220SF_LAUNCHXL_release_ccs' contains build-errors.
Build stopped..