Part Number: CODECOMPOSER
Other Parts Discussed in Thread: BOOST-CC2564MODA, CC3200AUDBOOST
Tool/software: Code Composer Studio
Hey all,
I am extremely new to this world. I am starting to experiment and play around with the MSP432P401R, with the BOOST-CC2564MODA. At the moment I have a simple goal of uploading an example to this and being able to connect to it. I understand I'll need other BoosterPacks to do audio functions and such, that will come at a later time.
My current issue is in Code Composer Studio. I have imported SPPDemo into IDE following the SWRU453B user guide. I opened the properties and made sure the correct LaunchPad was selected, I tested the connection, and made sure the checkbox to automatically configure the target-configs was selected. When I build the file I get the following errors:
gmake: *** No rule to make target 'C:/Users/frali/workspace_v9/Main.c', needed by 'Application/Main.obj'.
gmake: *** No rule to make target 'C:/Users/frali/workspace_v9/SPPDemo.c', needed by 'Application/SPPDemo.obj'.
gmake: *** No rule to make target 'C:/Users/Bluetopia/btpskrnl/BTPSKRNL.c', needed by 'Bluetopia/btpskrnl/BTPSKRNL.obj'.
gmake: *** No rule to make target 'C:/Users/Bluetopia/btpsvend/BTPSVEND.c', needed by 'Bluetopia/btpsvend/BTPSVEND.obj'.
gmake: *** No rule to make target 'C:/Users/Bluetopia/btvs/BTVS.c', needed by 'Bluetopia/btvs/BTVS.obj'.
gmake: *** No rule to make target 'C:/Users/Bluetopia/hcitrans/HCITRANS.c', needed by 'Bluetopia/hcitrans/HCITRANS.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/MSP-EXP432P401R/CC3200AUDBOOST.c', needed by 'Platforms/MSP-EXP432P401R/CC3200AUDBOOST.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/MSP-EXP432P401R/HAL.c', needed by 'Platforms/MSP-EXP432P401R/HAL.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/MSP-EXP432P401R/ccs/msp432_startup_ccs.c', needed by 'Platforms/MSP-EXP432P401R/ccs/msp432_startup_ccs.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/cpu.c', needed by 'Platforms/driverlib/cpu.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/cs.c', needed by 'Platforms/driverlib/cs.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/flash.c', needed by 'Platforms/driverlib/flash.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/gpio.c', needed by 'Platforms/driverlib/gpio.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/i2c.c', needed by 'Platforms/driverlib/i2c.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/interrupt.c', needed by 'Platforms/driverlib/interrupt.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/pcm.c', needed by 'Platforms/driverlib/pcm.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/rtc_c.c', needed by 'Platforms/driverlib/rtc_c.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/sysctl.c', needed by 'Platforms/driverlib/sysctl.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/systick.c', needed by 'Platforms/driverlib/systick.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/uart.c', needed by 'Platforms/driverlib/uart.obj'.
gmake: *** No rule to make target 'C:/Users/Platforms/driverlib/wdt_a.c', needed by 'Platforms/driverlib/wdt_a.obj'.
gmake: Target 'all' not remade because of errors.
The directory it created for the target-configs is incorrect. I was under the impression it decides the locations based on the LaunchPad selection, which is why I made it a point to test my connection to ensure I had the right thing selected, but the directories on my computer are incorrect. Has anyone encountered this before? I wasn't able to find much searching for this issue. Hopefully it is a simple mistake!
Thanks