This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Resource Explorer is unable to connect to the internet. Not connected to the cloud server. Working in offline mode.

Part Number: CC2640R2F


Tool/software: Code Composer Studio

Hello!

My Resource Explorer is unable to connect to the internet.

Message: "Not connected to the cloud server. Working in offline mode."

I tried all this tips, but there is no result:

Ensure the setting is correct by performing the following steps:

  • Open the Preferences dialog (menu Window --> Preferences)
  • Type 'proxy' in the search box
  • Select 'Network Connections'
  • Under 'Active Provide', select 'Native'
  • Click OK
  • Close and restart CCS twice

Also try deleting the tirex-localserver-<version> folder found in C:\Users\<Userid>\ti and restarting CCS.

Another potential issue is that if there is an extra "node" process running. Close Resource Explorer. Check Task Manager or Activity Monitor and look for node. If one is running, kill it. Start Resource Explorer.

What can be sourse of the problem?

I attach .log (from c:\css8\.metadata\) and tirex-2019-07-06.log (from c:\Users\Alexandr\ti\tirex-localserver-3.6.5\.logs\)

css.zip