Tool/software: Code Composer Studio
Hi all,
I am quite new to Texas Instruments and CCS and I am struggling with the following:
The USB JTAG connector on my Sitara AM437x EVM broke off and thus connecting to the target via this port can not be done. I understand from the hardware user guide that XDS100V2 Emulation can be done via the UART and you should thus be able to connect to the target via the USB UART port. I am however strugling to make a connection to the target from CCS.
When I test the connection from the target configuration file, the following error message appears (connection selected as XDS100v2 USB debug probe and board selected as EVMAM437x):
I think a possible cause might be that there is no driver installed for the AM42xxv1.2 device (from device manager). If this is the cause of error, where can I find the driver to install on the host PC, otherwise any assistance would be appreciated!
Thanks in advance!