Part Number: TMS320C28346
Other Parts Discussed in Thread: CCSTUDIO, ENERGYTRACE
Tool/software: Code Composer Studio
Dear TI Support,
I recently transitioned from CCS v5.1.1.00031 to CCS v8.3.0.00009 and began experiencing a memory leak on the host PC. While CCS V8 is open the PC memory usage begins to creep higher. Closing CCS does not clean up the leaked memory. This will continue each time CCS is run until low memory warnings appear. Restarting the PC cleans the memory up and the process starts over. This appears to be related to two processes CCS V8 uses, cmd.exe and conhost.exe. These processes can be stopped by going to the Startup and Shutdown options and disabling all plugins. This will stop the leak while CCS is open and static, but when launching the debugger, the leak returns because the debugger starts and stops conhost.exe. Also, disabling the plugins causes some behavioral issues when running the debugger. CCS V5 running on this same PC did not exhibit this issue.
Best Regards
Ken Walker